What Are Low Power RF Terminations?
Key Takeaways
- Low-power RF terminations prevent signal reflection and interference
by absorbing energy at unused or switched ports in RF systems.
- They match the system’s characteristic impedance (usually 50 Ω), which maintains signal integrity by avoiding mismatch and reflected waves.
- Common applications include test and measurement setups, MIMO arrays, directional couplers, and switching networks where unused paths need termination.
- Multiple connector types and frequency ranges are supported, with increasing availability for millimeter-wave applications above 40 GHz.
- Proper termination ensures optimal performance and protects sensitive receivers and test instruments.
How Low Power RF Terminations Work
Low-power RF terminations function as matched loads designed to absorb RF energy and dissipate it as heat. They are engineered to match the characteristic impedance of the system, typically 50 ohms so that signals reaching the termination are fully absorbed rather than reflected. Internally, these terminations use precision resistive elements housed in a compact form factor, optimized for low power handling and wideband frequency performance. By eliminating reflections, low-power RF terminations help preserve clean signal behavior in RF and microwave circuits.
Common Use Cases for Low Power RF Terminations
Low-power RF terminations are widely used in test and measurement environments to terminate unused instrument ports and improve measurement accuracy. They are also essential in RF switches, directional couplers, and power dividers, where inactive ports must be properly terminated to prevent signal leakage. In modern communication systems, including MIMO and beamforming networks, low-power terminations ensure inactive signal paths do not degrade overall system performance. They are commonly used in laboratory setups, development platforms, and low-power RF signal chains.
Types of Low Power RF Terminations and Connectors
Low-power RF terminations are available in a variety of connector types to support different system interfaces and frequency ranges. Common connector options include SMA, SMB, SMC, SMP, SSMC, and N-type for lower frequencies, as well as precision connectors such as 3.5 mm, 2.92 mm (K-connector), 2.4 mm, and 1.85 mm for high-frequency and millimeter-wave applications. These terminations are offered in broadband and narrowband designs, with varying VSWR and frequency specifications to meet specific system requirements.
There are often occasions with RF signal chains where it is desirable to prevent the RF energy in that signal chain from either continuing along the signal chain or from exiting a given port. Given the nature of RF transmission lines, a simple short or open port will result in undesirable reflections and even signal emissions. Hence, it is often crucial to use RF Terminations to safely and securely absorb the excess signal energy while protecting other components in the signal chain from potentially harmful reflections that could cause interference or even damage. An example of this is when the transmission of a radar signal needs to abruptly stop by the time required to shut down the RF signal would take longer than the desired shut-off window. In this case, a switch can be placed in the transmission signal chain that redirects the output of the transmitter to a termination.
For legacy radars, the RF termination used in a radar application would need to be very high power. With the growing prevalence of smaller and more portable radar systems and communication systems, there is a growing need for Low-Power RF Terminations. A couple of factors are leading to this. With multi-input multi-output (MIMO) and beamforming technology there are typically many more signal paths feeding antenna elements than with previous radar and communication technologies that used a single higher power signal path. With a multitude of lower power signal paths, it is now possible to terminate these paths with low-power RF terminations. However, the higher number of signal paths also means that there needs to be a larger number of terminations available to terminate these ports.
Low power RF terminations are also extensively used with test and measurement applications. Many pieces of RF test equipment have exposed ports and benefit from having quality Coaxial Terminations at those ports. Moreover, there are many components and devices commonly used in RF tests that require RF terminations for some test setups, such as with directional couplers where only either the forward or reverse signal is needed.
As there is a plethora of various coaxial connector types, there are RF terminations made with each coaxial connector type. This includes push-connect type coaxial connectors, such as SSMC, SMP, SMC, SMB, etc.
With the growing interest in developing upper millimeter-wave technologies, there is a rising need for RF coaxial terminations that reach beyond 40 GHz. This is why 3.5 mm, 2.92 mm, 2.4 mm, and 1.85 mm are becoming increasingly available.
FAQs (Frequently Asked Questions)
1. What is an RF termination?
A: An RF termination is a matched load designed to absorb RF signals and prevent reflections in a transmission line. It typically matches the system's impedance (e.g., 50 Ω) to minimize signal distortion.
2. Are low-power RF terminations used?
A: They are used to terminate unused ports, switch paths, or test equipment interfaces in RF systems, ensuring that excess signal energy is absorbed rather than reflected into the system.
3. How do low power and high-power terminations differ?
A: Low power terminations handle lower wattage signals (often in the 1 W to 5 W range), while high power terminations are designed for much higher power levels and may include heat sinks or other cooling features.
4. Do low-power terminations come in different connector types?
A: Yes. They are available for a wide variety of coaxial connector interfaces, including SMB, SMC, SMP, and SSMC, and are also compatible with high-frequency connectors used above 40 GHz.