A 90 Degree Hybrid Coupler is a one of the few hybrid coupler types, the others include 180 degree hybrid couplers and 0 degree hybrid couplers. 90-degree hybrid couplers are also known as quadrature couplers/hybrids, as any signal injected into any port will result in two 90 degree out-of-phase signals present on the other two ports. The output signals in a 90-degree hybrid coupler are typically split evenly between the two output ports, meaning that the signal energy is 3dB (half signal strength) less at the outputs than the inputs, but otherwise identical except for being out-of-phase by 90 degrees.
Related articles
Peter McNeil | Aug 09, 2022 | RF Couplers
A RF Coaxial Hybrid Coupler is a type of RF coupler that essentially behaves as an equal power splitter while also creating a phase shift between the two ports. RF hybrid couplers are generally distinguished by the degree of the phase shift, be it 0 (no phase shift and just a 4-port directional coupler), 90, or 180. A unique attribute about RF hybrid couplers is that the phase shift between the coupled ports is broadband. Other important metrics of a hybrid coupler are the phase balance, amplitude balance, and the extent of the isolation between the coupled (output) ports.
As such, RF hybrid couplers are a special case of four-port directional couplers, which is specifically designed to have a 3dB coupling, or equal power split, and 90- or 180-degree phase shift between the coupled ports. Like with a four-port directional coupler it is critical for the design of an RF hybrid coupler to be as symmetric as possible. The accuracy of a hybrid coupler phase shift is only good to a certain bandwidth. This is also true for the amplitude balance, phase balance, and isolation. Hence, a hybrid coupler is generally only specified over a broad, but fixed, bandwidth based on what is considered a reasonable threshold for these metrics.
180-degree Hybrid couplers are sometimes realized using a rat race coupler designed in a specific way to realize the desired coupling and phase shift between the ports. It is important in the design of a hybrid coupler to achieve low VSWR, isolation, and phase/amplitude balance, which is often why a rat race coupler design is chosen. Another method is to modify a branchline coupler designed as a 90-degree hybrid and adding a 90-degree section to one of the branchline coupler ports.
A use case of hybrid couplers is to enhance the isolation between two RF signal paths that cross each other. Other methods of achieving this could be to use an airbridge or a wire bond cross over to provide physical isolation. A planar hybrid coupler, on the other hand, can be used to isolate two crossed paths in-plane. All that is required is to cascade two hybrid couplers together, and the four-port network that results has isolation between the two RF paths. It should be noted that this method does limit the bandwidth of the signal paths and does require significant board or die real estate.
Learn more about 90 Degree Hybrid Couplers in this post by Fairview Microwave: /content/fm/en/blog/archives/2022/what-is-a-90-degree-hybrid-coupler.html
Peter McNeil | Feb 05, 2025 | RF Couplers
Key Takeaways
- Defense-grade RF couplers must handle extreme environmental stresses including shock, vibration, humidity, altitude/pressure variations, corrosion, and wide temperature swing conditions often far beyond typical commercial applications.
- High power handling capability is critical: couplers used in radar, satellite communications, or high-power transmit paths may need to manage hundreds to thousands of watts, both CW and pulsed, without performance degradation.
- Wide frequency bandwidth is often a requirement for defense systems that may operate across C-band, X-band, Ku-band or beyond, so a coupler must maintain coupling consistency, isolation, and VSWR over a broad spectrum.
- Materials and construction must meet or exceed military specifications (MIL-spec) for plating, connectors, sealing, and mechanical joints, for example, corrosion-resistant plating to prevent degradation in marine or high-humidity environments.
- Proper coupling quality means high directivity and isolation, minimizing signal leakage, or reflection. This is vital for accurate signal sampling, monitoring, or measurement in defense communication and radar systems.
Why Standard RF Couplers Often Fall Short in Defense & Aerospace Usage
Standard commercial RF couplers are designed for controlled environments such as labs, indoor communication setups, and general-purpose RF testing. Defense and aerospace applications, however, operate in conditions far more demanding than what these components are typically rated for. High vibration levels, extreme temperatures, rapid pressure changes, shock loads, and long-term exposure to humidity or corrosive elements can quickly degrade a commercial-grade coupler.
Additionally, military communication, radar, and EW (Electronic Warfare) systems require exceptional stability and accuracy over wide frequency ranges. Commercial couplers often exhibit performance drift under thermal stress, limited power handling capability, and inconsistent coupling values outside their nominal specifications. These limitations can impair signal sampling, degrade system performance, and compromise mission-critical reliability making standard couplers unsuitable for defense-grade deployments.
Coupler Types for Defense Applications: Waveguide vs Coaxial vs Directional
Defense systems rely on a variety of coupler technologies based on power levels, frequency bands, and environmental constraints:
Waveguide Couplers
Waveguide couplers are commonly used in radar, airborne systems, and high-power microwave applications. Their inherently low loss and high-power handling make them ideal for X-band, Ku-band, and Ka-band systems. They also offer excellent environmental resistance due to their rugged metallic structure.
Coaxial Couplers
Coaxial couplers are chosen when systems require compact size, moderate power handling, or compatibility with existing coaxial architectures. For defense environments, they must feature reinforced bodies, corrosion-resistant plating, hermetic or weatherproof sealing, and MIL-spec connectors to survive harsh climates and shock/vibration loads.
Directional Couplers
Directional couplers provide accurate sampling of forward or reverse power and are essential in radar calibration, VSWR monitoring, jamming systems, and antenna performance verification. In defense applications, they require high directivity, stable coupling factors across wide bandwidths, and ruggedized construction to maintain measurement accuracy even under thermal or mechanical stress.
There are many instances in military/defense, aerospace, space, and naval applications where there is a need for sampling signals from high power transmission paths or monitoring the frequency of high-power signal paths. In these cases, the best RF component for the job is often an RF coupler. However, not all RF couplers are designed for extreme environmental applications indicative of the requirements for defense applications.
For instance, many RF couplers have coaxial connector ports either for the primary signal paths or the coupled ports. If the coaxial connector ports are coaxial types that use dielectric spacers, it may be that the dielectric material used can’t sufficiently perform under extreme temperature ranges specified for military grade coaxial connectors. Other environmental features include corrosion resistance, shock, vibration, humidity, altitude/pressure, etc.
Generally, standard waveguide flanges can meet all of these requirements, possibly with the exception of corrosion resistance. This is why many waveguides meant for defense applications are gold plated; this helps prevent corrosion while still maintaining high conductivity for low loss performance. A common standard for body plating specifications for waveguide couplers is MIL-DTL-5541.
Even with waveguide couplers, if the attachment methods of the coupled ports aren’t designed to withstand shock and vibration, the joint between the main waveguide and coupled waveguide may degrade or even fail. Hence, it is often imperative to ensure that even waveguide couplers are designed to meet MIL-Spec standards for ruggedness. For altitude/pressure performance, couplers often need to be sealed, either hermetically or with epoxy, to prevent outgassing or debris ingress to meet defense standards.
RF couplers designed for defense applications also tend to be specified to operate over certain useful frequency ranges and power levels for defense use cases. Examples of this include RF directional waveguide couplers designed to operate from 100s to 1000s of Watts and in key radar frequency bands, such as C-band, X-band, Ku-band, etc. These couplers will often have high peak and continuous wave (CW) input power ranges specified, as radar applications tend to have high peak power outputs.
All of these factors considered together likely indicate that a RF coupler has been designed to meet defense applications, even if it is not explicitly identified as such.
Recommendations
For defense and aerospace RF systems, selecting the right coupler requires a strategy that balances electrical performance, ruggedness, and long-term reliability. Engineers should always choose MIL-spec–qualified waveguide or coaxial couplers when operating in high-power or mission-critical environments, as these units are designed to withstand harsh thermal, mechanical, and environmental stress. It’s also recommended to prioritize couplers with high directivity and stable coupling values across wide frequency bands to ensure accurate signal sampling and system diagnostics.
When integrating into airborne, naval, or mobile platforms, opt for models with hermetic sealing, corrosion-resistant plating, and vibration-rated construction to prevent moisture ingress and mechanical fatigue. For systems that involve pulsed radars or EW transmitters, selecting couplers with robust peak power handling and low insertion loss is essential to avoid electrical breakdown. Finally, engineers should perform regular calibration checks and preventive maintenance on couplers to monitor drift, verify connector integrity, and ensure system readiness under demanding operational conditions.