Fairview Microwave Launches Series of Step Attenuators with Pinpoint Accuracy
NEWS RELEASE
New Line of Step Attenuators Offers Wide Variety of Attenuation Ranges
IRVINE, Calif. – Fairview Microwave, step attenuators for instrumentation, precision measurements, prototyping and characterization production system and other applications requiring precise control of signal levels.
Fairview Microwave’s new step attenuators feature attenuation accuracy of +/- 5 dB, making them ideal for use in high-reliability applications demanding accurate adjustment of attenuation values.
Additional superior performance characteristics for the step attenuators includes 1dB maximum insertion loss and a maximum VSWR of 1.4:1.
These high-reliability step attenuators offer wide coverage and high power with an operating frequency range up to 18 GHz and a 2W power rating.
Fairview‘s new line of step attenuators provide SMA and N-type connectorized designs and attenuation step sides ranging from 1 dB to 99 dB depending on the model.
“Fairview Microwave’s expansion of step attenuators guarantees our customers achieve reliable performance for their extreme precision applications,” said Steven Pong, Senior Product Manager.
Fairview Microwave’s new step attenuators are in-stock and ready for immediate shipment with no minimum order quantity.
For inquiries, Fairview Microwave can be contacted at +1-972-649-6678.
About Fairview Microwave:
A leading supplier of on-demand RF and microwave products since 1992, Fairview Microwave offers immediate delivery of RF components including attenuators, adapters, coaxial cable assemblies, connectors, terminations and much more. All products are shipped same-day from the company’s ISO 9001:2015 certified production facilities in Lewisville, Texas. Fairview Microwave is an Infinite Electronics brand.
About Infinite Electronics:
Based in Irvine, Calif., Infinite Electronics is a global electronics supplier, offering a broad range of components, assemblies and wired/wireless connectivity solutions, serving the aerospace/defense, industrial, government, consumer electronics, instrumentation, medical and telecommunications markets. Infinite’s brands include Pasternack, Fairview Microwave, L-com, MilesTek, ShowMeCables, NavePoint, INC Installs, Integra Optics, PolyPhaser, Transtector, KP Performance Antennas, RadioWaves and Aiconics. Infinite Electronics serves their customer base with deep technical expertise and support, with one of the broadest inventories of products available for immediate shipment, fulfilling unplanned demand for engineers and technical buyers. Infinite Electronics is a Warburg Pincus portfolio company.
###
Press Contact:
Peter McNeil
Fairview Microwave
17792 Fitch
Irvine, CA 92614
(978) 682-6936