The Argument for the 90 Degree Coax Adapter
It is often necessary when connecting diverse systems and components to use a 90 degree coax adapter to mate between connections with differing coaxial connector standards. Like with all RF coaxial applications, RF coaxial adapters including a 90 degree coax adapter can be instrumental from the field and production to the laboratory.
Key Takeaways
A 90° coax connector adapter is often chosen where physical space or routing constraints demand a right-angle connection rather than a straight one
Mechanical advantages include more compact installation, reduced cable-bend stress, improved fit in tight panels, or chassis.
However, using a right-angle adapter may influence RF characteristics (additional connector transitions, possible slight increase in VSWR or insertion loss) and must be evaluated in high-performance systems.
The decision to use a 90° adapter should weigh both mechanical/space benefits and the RF system's performance requirements.
Proper selection, installation, and specification review (frequency limits, connector type, power rating, VSWR) ensure the adapter delivers its intended benefit without compromising signal integrity.
These versatile adapters can be used with coax cable assemblies with similar of different connector ends that have already been purchased. The avoids have to buy new cable assemblies. Right angle coax adapters feature in-series connectors (the same connectors ) or between series (different connectors) versions to address every application imaginable.
We offer a wide array of off-the shelf right angle coax adapters to address a range of applications.
The list below highlights these angled adapters:
- Right Angle 1.85 mm Coaxial Adapters (Miter)
- Right Angle 2.4 mm Coaxial Adapters (Miter)
- Right Angle 2.92 mm Coaxial Adapters (Miter)
- Right Angle SMA Coaxial Adapters (Miter)
- Right Angle 1.85 mm Coaxial Adapters
- Right Angle 2.92 mm Coaxial Adapters
- Right Angle 3.5 mm Coaxial Adapters
- Right Angle 4.3-10 Coaxial Adapters
- Right Angle 7/16 DIN Coaxial Adapters
- Right Angle BNC Coaxial Adapters
- Right Angle C Coaxial Adapters
- Right Angle HN Coaxial Adapters
- Right Angle LC Coaxial Adapters
- Right Angle MHV Coaxial Adapters
- Right Angle N-type (Type N) Coaxial Adapters
- Right Angle QMA Coaxial Adapters
- Right Angle SC Coaxial Adapters
- Right Angle SHV Coaxial Adapters
- Right Angle SMA Coaxial Adapters
- Right Angle SSMA Coaxial Adapters
- Right Angle TNC Coaxial Adapters
- Reverse Polarity Right Angle SMA Coaxial Adapters
- Reverse Polarity Right Angle TNC Coaxial Adapters
- Radius Right Angle 2.92 mm Coaxial Adapters
- Radius Right Angle Type N (N-type) Coaxial Adapters
- Radius Right Angle SMA Coaxial Adapters
- Radius Right Angle TNC Coaxial Adapters
These coax adapters are essential in clustered interconnect environments where a typical coaxial connector and cable attachment won’t allow for sufficient clearance for insertion or extraction. Moreover, using a right-angle adapter can eliminate the need for a straight adapter on either the port or cable assembly side of the adapter, which may further reduce the overall interconnect footprint.
Recommendations
Evaluate physical installation constraints early—if space is tight or panel depth limited, plan for a 90° adapter rather than forcing routing compromises.
Match the adapter’s frequency range, power handling, connector type and VSWR specification to your RF system’s requirements (especially in high-frequency or PIM-sensitive setups).
When using 90° adapters, keep cable runs as short and direct as possible to minimize additional loss or reflections introduced by the angle.
Consider the adapter’s body material and durability, especially in environments with vibration or mechanical stress, since right-angle adapters may see load in different directions.
Include the right-angle adapter’s impact on your RF budget (loss, return loss, PIM) just as you would any transition or connector.
As with typical coaxial adapters, there are as many right-angle coaxial adapter types as there are coaxial connector standard combinations. However, there are also additional types of right-angle adapters to accommodate different performance requirements. Traditional RA adapters are designed to provide the minimal footprint to perform a right-angle transition. This is often at the sacrifice of performance and possibly even maximum frequency of operation. There is a solution to this however, but it involves bending a rigid cable around an acceptable radius for the maximum frequency of operation. These radius right angle, or swept radius right angle, 90 degree coax adapter variations tend to be better performing than their hard right-angle counterparts, but also tend to be more expensive and larger than typical right angle adapters. Other 90 degree coax adapter types include reverse polarity (RP) types, but these are often limited to SMA and TNC connector standards, as those are the most common found with RP configurations.